cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Tool to obtain the drive / motor diagram online?

Tool to obtain the drive / motor diagram online?

ericvergara
Occasional Contributor

Hello,

We have a customer that is using the ctrlX Core with seven ctrlX Drive,

This customer is used to work with B&R and he claims that they have a tool to calculate the drive and motor diagram and also the cycle points, so he can check if the mechanics and the drive and motor are accordingly sized,

I know that with the IndraSize we can do it offline but whit this tool they can do it connected to the real machine and with the real cycle points,

So, do we have something similar to this?

Thanks,

ericvergara_0-1677490212353.png

2 REPLIES 2

Drives_Uwe
Community Moderator
Community Moderator

A look on the behavior of the mere motor drive combination inside the ctrlX DRIVE Engineering tool is possible, see (one can look on the torque or power over speed characteristics over the complete speed range):

Drives_Uwe_0-1678186834608.png

 

To check as well the application cycle one needs to
- create a scope file
- export this scope file to Excel (".csv"-file)
- insert this file into the sizing tool IndraSize
- and check the working points

See:

Drives_Uwe_1-1678187217378.png

Drives_Uwe_2-1678187381295.png

Drives_Uwe_3-1678190315241.png

Drives_Uwe_1-1678208429984.png

Drives_Uwe_0-1678208398308.png

 

 

 

 

ericvergara
Occasional Contributor

Many thanks 😊

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist