Could we use XCS1 converters with 1x230V ?
Solved! Go to Solution.
1-phase operation (L1-N) are not possible.But a operation with 3x230V (L1-L2-L3) are possible. The derating is then 2.5%/V, so we will then still supply approx. 57.5% of the nominal power or peak power.
In the meantime an operation of XCS2 converters at single phase 230 V is possible. See as well actual projecting documentation:
https://www.boschrexroth.com/documents/12605/25199765/R911386579_08.pdf/03946283-8054-6df2-4721-cc31...
When will 1-phase 230V AC be implemented into IndraSize for the XCS2 ctrlX drives?