08-28-2024 05:35 PM
Hello,
I am in the process of testing SSI feedback connection/functionalities with ctrlX DRIVE. It seems to me that the firmware version 5V04 seems does not recognize SSI encoder. I have used Balluff BTL5-S171B and SICK AFM60E encoders for the test. Both encoders are working with IndraDrive but ctrlX DRIVE with firmware version 5V04 would not recognize it. When the firmware is updated to 6V02 then the SSI feedback is recognized and track the correct distance.
If someone can verify this issue that will be great.
Thanks
08-29-2024 11:27 AM