05-01-2024 07:12 AM
For the XG31 IO the parameters for reading inputs is P-0-0307 and P-0-0313 for writing outputs.
With the DA option on ctrlX drive Plus, are the same parameters used (ie more bits of the same parameters)? Or are there additional parameters?
Are the same parameters used for XCS2-F connector XG31?
Solved! Go to Solution.
05-02-2024 09:00 AM
Always parameters P-0-0307 and P-0-0313 are used to show the input/output state, no matter if ctrlX DRIVE, ctrlX DRIVE with additional DA option or XCS2-F is used.