04-12-2022 03:46 PM
I am having trouble with the parameter P-0-2054, Operational performance, motor. This parameter states to give an estiamtion of the total travelled distance of the axis in meter. I tried to test the parameter by travelling long distances by high and low speed with the axis, but the value of the parameter did not change at any moment.
Also a quick look on the parameters "P-0-2051, Operating hours counter, motor" and "P-0-2053, Mechanical operating data, motor" seemed like they are not changing while or after any movement.
Is there a setting needed to activate those paramters? Or is this not how these parameters function?
Solved! Go to Solution.
04-13-2022 07:58 AM
The parameters should work directly. There is no activation parameter or similar present.
Please send your saved parameter file (format: all parameters) to check if anything else is weird.
04-20-2022 11:29 AM
04-26-2022 10:07 PM
Please change to latest firmware version AXS-V-0308.00.NN
There it works as I checked today.
06-02-2022 10:21 AM
We have checked the parameter on different Drives with the firmware version AXS-V-0308.00.NN and also the second latest firmware version. In both cases the value of the P-0-2051, Operating hours counter, motor" and "P-0-2053, Mechanical operating data, motor" are constant values >0 and stay at this value even if the axis is moved. Is there any Bug known or setting that disables the functionality of these parameters?
06-03-2022 12:47 PM
As said works in my setup with Firmware AXS-V-0308N-NN-00 both with MSK and MS2N motors:
06-03-2022 12:56 PM
But looking into the saved parameters of you it seems to work, see:
06-15-2022 02:32 PM
Thank you for checking our used Parameters.
The operating hours(P-0-2051) works as expected. The problem is now only the parameter that states the travelled distance of the motor(P-0-2054, Operational performance, motor).
I had 2 ideas why this value seems not to work.