FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
11-02-2022 03:48 PM
Hello,
A customer asked how to mirror the lightpipe function of the drive in their hmi.
I've tried to find a parameter that shows the current lightpipe color without success.
It is documented in the manual wich color means what, but seems like reinventing the wheel.
Anyone has done this in some way?
Solved! Go to Solution.
11-03-2022 12:28 PM
A meaningful display of the drive diagnostics should be realized via parameters S-0-0390 or S-0-0095.
11-03-2022 12:36 PM
The light pipe control can be seen in parameter P-2990.0.7.
With the double-axis module, the axis with the smallest value (= highest priority) is displayed.
see example
11-07-2022 10:35 AM - edited 11-07-2022 10:38 AM
11-08-2022 08:22 AM
This is intentional!
Only "important" parameters can be transmitted in the cyclic channel.
It is not possible to transfer the P2909.0.7 into the AT, not even in the future!
For diagnostics please configure S-0-0390 into the AT!
11-17-2022 10:06 AM
03-16-2023 03:25 PM
The lightpipe status (P-0-2990.0.7) will be able to be read in the cyclic channel starting with firmware 03V16 !