02-28-2023 02:47 PM
We drove into problems updating a ctrlX drive. F8115 was generated.
Update process seems to be fullfilled without a problem. After updating a XCD1-W2323 from V-0210 to V-0308 (or V-0314) we get drive ready (blue lightbar is good) and there is no failure.
After reboot it seems that something is wrong.
What’s wrong ? Did we used the wrong Firmware file ?
Solved! Go to Solution.
02-28-2023 02:54 PM - edited 02-28-2023 04:23 PM
It seems like the problem is the generation_1 ctrlX drives. I found this on the Forum ... 🙂
The XCD1 is not suited for the V-03.. firmware. Version V-03.. will only work with XCD2, or other variants of the X__2 generation.
It should have helped if during the firmware update a pop-up should appeared with
"sorry my friend, this will not work due to the hardware version"
Right now the firmware is uploaded, and after bootup the drive sees that the firmware is not compatible with the drive resulting F8115.
Loading the V-02.. Firmware back into the drive resulted in a error free ctlX drive again.
02-28-2023 05:13 PM
Good, that you could sort it out by yourself.