Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

F2037 Excessive position command difference error over a certain speed.

F2037 Excessive position command difference error over a certain speed.

CsTemesvari
Member

Hi,

I'm trying program a system which contains the following items:
ctrlX Core X3: 1.20
Motion App:  1.20
PLC App: 1:20
HMS01 Single axis inveter

I'm using the CXA_MotionInterface. I can start the drive as needed, but after a certain speed 2000rpm to be exact, the drive stops with F2037 Excessive position command difference error. Under that speed everithing works fine. I tried to change the S-0-0091 parameter of the drive to a higher value as the help suggest but nothing works for me.
I checked all the limit values in drive engineering and also Motion app. Everywhere I have higher values than 2000 rpm. (see the attached photos).
I also uploaded the drive parameters.
Any help would be appreciate

Thanks, Csaba

6 REPLIES 6

stefanAT_ctrlX
New Contributor

Hello Csaba,

did you also check the acceleration bipolar limit S-138 ? Maybe here is the limit ?

stefanAT_ctrlX_0-1695192824148.png

 

Regards, Stefan

Drives_Uwe
Community Moderator
Community Moderator

Please have a look to parameters P-0-0010 and P-0-0011 in the error case F2037

Drives_Uwe_0-1695311943339.png

My guess is that on the control system you have not chosen modulo scaling whereas on the drive side it is chosen. See:

Drives_Uwe_1-1695312143675.png

Note: Normally it is recommended to set the maximum travel range to the same value as the modulo value. So in here instead of 5000° you should enter 360° as well.

That - inconsistency of scaling in between drive and control - may explain why it is going wrong.

CsTemesvari
Member

Hi,

Thanks for your answer, but I use way smaller acceleration and deceleration.

Hi,
Thanks for your reply, I can try this next week. I will give a feedback as soon as possible.

Are there any news or can this topic be closed?

Sorry for a really late response, but I could not do any test until now. Somehow I was look over the most obvious parameter. (red arrow)
Thanks for all of your help!

2023-11-24_11h21_44.png

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist