05-19-2023 09:45 AM
Hello,
A customer is going to make 3 machines with external encoder functionality with measuring wheel and asks me if this Encoder can work without problems with the CtrlX Drive and the additional EC.
It is an Endat 2.2 Encoder, because of the interface type it could work without problems and it is compatible with the EC of the CtrlX Drive.
Is there any recommendation of a specific model of encoder?
Thanks in advance.
Solved! Go to Solution.
05-19-2023 02:37 PM
The encoder from the specification fits to our EC interface. So it should work.
05-22-2023 09:41 AM
Thanks Drives_Uwe.