Error when activating "Dynamization source for safe inputs at the XG44 interface"

Error when activating "Dynamization source for safe inputs at the XG44 interface"

D_Wengeler
New Poster

During the commissioning of my drive, I wanted to implement STO function via two safe inputs. I would like to use two terminals as dynamization outputs and I get the following error message when I try to set the checkmark "Dynamization source for safe inputs at the XG44 interface":


The value of the property Local safe interface cannot be determined safely.

Value of pass A:
S-0-0000.0.0_bit0

Value of pass B:

To remove the error, restart criX DRIVE Engineering.

I obviously restarted ctrlx DRIVE Engineering but this did not solve the problem. I have also reset the drive, used a different version of ctrlx DRIVE Engenieering and also tried a different computer.

What am I doing wrong? Is this a known behavior?

ctrlX Drive Engineering Version 1.20.0
Controller XCS2-W0023ARN-02AX3M5NNET-S0308N2NNNN3NN - AT1
Firmware FWA-XD1-AXS-V-0308N-NN.05
Motor axis MS2N03-B0BYN-CMSG1-NNNNN-NN - A

2 REPLIES 2

PADE
Established Member

Hi, @D_Wengeler

just comment. I have tested this function quite recently without any problem.

But I have newer ctrlX Drive Eng. and newer FW in drive. (Also tested without integrated X3 core).

Do you need to stay in version 03V08 or you can update to newer version? I would recommend that.

BR, P.

DepecheMode
Long-established Member


Please switch to ctrlX DRIVE Engineering 1.30.0 and test it again.
The setting works for me on
XCD2-W2323ARN-02NETM5ECNN-S0308N2TX1P3NN
FWA 0308.05

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist