09-25-2023 01:10 PM
Hi
Can you help me with pin assignment of M17 connector (Resolver encoder) on this servo engine. We ordered original cable but it will came in 3 weeks. For now i need selfmade cable for testing. It is impossible to find information cable pinout. I just found where to solder cables on D-sub connector.
Solved! Go to Solution.
09-26-2023 08:07 AM
Here you are:
09-27-2023 09:03 AM
09-28-2023 07:50 AM
Yes, sorry, you are right. there is a misprint in the E PLAN document:
+ UB on the motor side is not on pin 1 but on pin 2. --> So connect pin 15 on the drive side with pin 2 on the motor side.
The rest of the plan is correct.
10-12-2023 08:39 AM
Hi thank you for your help, now it is working but i cannot find some parameters from this resolver. Indraworks need some parameters which i can't find DP/rev. I was trying to find it but i failed. It is parameter S-0-0602.x.3
Thank you