FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
09-20-2024 03:21 PM - edited 09-20-2024 09:35 PM
Do we have a similar table (shown below) for CtrlX drives? we need to know how how long the peak current can be substained? as per diff PWM.
09-23-2024 12:25 PM
With the help of IndraSize one can create the possible currents by yourself, see e.g. for XCS 90A
This is too much therefor the currents are reduced
Thus for 8 kHz PWM the proper value pair is: 28A continuous and 30,8 A peak for 10s in a 10 min cycle.