05-06-2020 01:02 PM
In the communication interface, is it multi-function? Can it be changed by parameter or set from display?
Solved! Go to Solution.
05-06-2020 03:19 PM
The functionality is similar to today.
The communication protocol used by interface can be changed by parameters (also possible from panel).
In the very moment only EtherCAT and sercos are available. In November 2020 ProfiNET is planned to be added as well. See Roadmap.