FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
08-02-2023 12:02 PM
Hello,
on an HCS drive, the second encoder works, when I transfer it to the CtrlX Drive.
there's an error.
HCS in mm and CtrlX in nm
Someone could me helping?
CtrlX:
FW: FWA-XD1-AXS-V-0308N-NN.03.fwa
Drive: XCS2-W0023ARN-02AETM5ECNN-S0308N2NNNN3NN
Solved! Go to Solution.
08-03-2023 06:14 AM
Hello
after this command error, please open S-0-0423 in the parameter editor to check which values are invalid.
Can you also send a complete parameter file saved with all parameters?
regards,
Stefan
08-03-2023 03:26 PM
Problem was fixed after changing the clock rate of the SSI encoder to 400 kHz.