01-07-2022 10:11 AM - last edited on 01-14-2022 08:39 AM by CodeShepherd
I installed the release version of November (V112) and still I have this problem seen twice.
After installing an app the operation mode button is greyed out. It was necessary to use the µSD-card to make the system up and running.
Is there another solution available?
Note: The system is not rebooting. Switching power off/on does also not help.
Solved! Go to Solution.
01-10-2022 09:03 PM - last edited on 01-14-2022 08:40 AM by CodeShepherd
Hello,
could you please point out in detail what happend? Wonder if I get the message correct.
Assuming you made a factory-reset using the uSD with the RM2111 Image to refresh the system. After that, the system was on RM21_11 level and the reboot and state switching worked fine, right?
What happend next?
Did you only load apps fitting to RM21_11? Just ones labeled with 1_12 instead of the RM2107related 1_10 versions?
Which app-handling is related to the trouble?
Did you operate with configurations based on old RM2107 ?
Please return with further details.
Bye!
01-14-2022 08:40 AM
Moved to own topic.
02-28-2022 09:57 AM
Any further news or can this topic be closed?