ctrlX Core X7 - what to expect from the Display Port?

ctrlX Core X7 - what to expect from the Display Port?

jacaré
Long-established Member

What do you get on screen when the ctrlX Core X7 is connected to a monitor?
Because it runs ctrlX OS, I assume all I get is boot information and afterwords a command line?
Can I run Apps with a GUI?

3 REPLIES 3

bostroemc
Occasional Contributor

I don't have an inside line on the official plans for the Display Port functionality on ctrlX CORE X7, but on generic devices running Ubuntu Core it is possible to install a display server like Ubuntu Frame and then run GUI applications within this server in kiosk mode.  Note that Ubuntu Frame supports the Wayland protocol.

A good introduction to this topic is given here.

The attached video shows a snapped Qt6 application running within Ubuntu Frame.  The application includes a live OPC UA connection to ctrlX CORE (backend open62541).  I've verified that the snap runs on an Intel NUC running Ubuntu Core 20.

Screenshot from 2023-02-27 15-57-03.png

 

 

 

 

 

jacaré
Long-established Member

This looks very promising. Still, I would love to hear the official plans for the Display Port.

Sophie
Community Moderator
Community Moderator

Hello jacaré....

the official plan is to have a concept for the display port for the ctrlX COREplus X7 until end of juli 23 and then to go in the implementation of this concept.

If you have use cases or expectations regarding the display port, that you would like to share with me, please contact me.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist