01-27-2023 11:57 AM - last edited on 01-30-2023 08:28 AM by CodeShepherd
Hi,
I use currently V1.18 of ctrlX core. I made the update a few weeks ago. Everything was ok: some standard apps deployed afterwards and I focused on own developments in node-red. Since 3 days I have following situation:
1) Around 17:00 I go home and system is left connected 24/7 to the power supply
2) Everyday in the morning:
See attached video
So I decided to restart by unplugging the power.
And following situation after restart:
Any ideas?
Is this a battery issue?
Kookoolinoo
* PS. The update from today incident - the only difference to the described above bahevior is that today I cannot see any logs.
And there are no logs at all even current logs are not collected. I played for a while in the wb gui I one log was generated which says:
27.01.2023 11:48:45.977 080F0410 Trace error web.common.loggerServer validation: Failed to write WLS_CMD_VALIDATE response: write unixpacket /var/snap/rexroth-deviceadmin/2142/auth-service/token-validation.sock->@: write: broken pipe
Solved! Go to Solution.
01-30-2023 09:05 AM
Moved to own topic from this thread.
The battery is only buffering the system time. As your log shows an actual date and time and your system is connected permanently to a power supply there should be no problem.
In standard the diagnostic log message are not persistent. You can change this setting for testing purposes or us a remote logging server.
09-30-2024 01:36 PM
Moved to own topic.