Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

X7 Label communication

X7 Label communication

JHU1XI1
Long-established Member

hello.

  Why are the encryption options missing(V1.20)

2023-11-20_15h02_19.png

2023-11-20_15h29_33.png

 How do I need to set up tag communication?

3 REPLIES 3

georkueh
Community Moderator
Community Moderator

Hi,

ctrlX CORE devices only allow encrypted PLC communication. So there's no need to show this setting. User may wonder how to disable this according to other CODESYS targets.

Hope this helps!

JHU1XI1
Long-established Member

This is because I need to communicate with a third-party HMI for tag communication. If the encryption is not cancelled, communication cannot be achieved. The HMI supports tag communication using the Codesys protocol.

georkueh
Community Moderator
Community Moderator

Hello,

CODESYS provides the PLC Handler, that allows encrypted communication. If the HMI supports CODESYS protocol, it must be based on the PLC Handler. So you should contact the HMI provider to use a PLC Handler that allows encrypted communication. I suggest, currently he is using an older version of the PLC Handler that did not allow encrypted communication.

 

kind regards

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist