Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Update and setup via SD card

Update and setup via SD card

Venzi_
Established Member

Hi,

Can I use the procedure for update and setup via SD card described here:

https://developer.community.boschrexroth.com/t5/Store-and-How-to/Update-and-setup-ctrlX-CORE-with-a-...

to update CPU running with rm21_11 to rm23_03?

Thanks,

Venzi

4 REPLIES 4

Marc-Smaak
Established Member

Yes, this is the easiest way but it will erase all your current settings including users. If you do not want this you can update through the GUI but must follow the order as documented in the releasenotes

Check: ctrlX CORE Runtime, Release Notes XCR-V-0120

From: https://docs.automation.boschrexroth.com/doc/3957395426/ctrlx-core-runtime-release-notes-xcr-v-0120/...

CodeShepherd
Community Moderator
Community Moderator

As mentioned in the how to and you can see in your ctrlX CORE with apps version 1.12 (RM21/11), for the setup mechanism minimum version 1.20 is needed.

So you can do an image update but creating a setup is not possible. On the old version. Also Backup/Restore between different version is quite not working in that state.
What could be used is exporting your active configuration (app data) and import them after updating. Beware that there could be some incompatibilities. See e.g. topic "Motion app hangs in Configuration/Running after booting"

Venzi_
Established Member

I am looking for a remote offline solution and unfortunately the configuration approach doesn’t work for me. I saw the statement in the how-to, but hoped that after the system image is replaced with the 1.20 version on the old Core, the setup (created on a 1.20 source) can be applied automatically after reboot from the SC card, because the old Core has then 1.20 already.

CodeShepherd
Community Moderator
Community Moderator

This is possible. See online documentation "Setup - Automatic setup application upon system start".

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist