FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
01-19-2021 04:31 PM
Is it possible to use the USB-C port from the application on the core? I would like to use this to read write data to a USB device.
Solved! Go to Solution.
01-21-2021 02:55 PM - edited 02-16-2021 08:29 AM
It is planned to have it via PLC and own apps available in the release RM21.07 (Version 1.10.x) of our system.
03-31-2022 09:18 PM
@CodeShepherd , is there an update to this? I see that the USB and SD card can be mounted, can it also be accessed from PLC application?
04-01-2022 07:22 AM
Like mentioned above this feature was already implemented.
You can find some information in the how to area for using libusb in your own snap.
See this post for how to mount and use external storage.
You can have a look to the official documentation for supported hardware like mentioned in this post:
ctrlX CORE Runtime, Application Manual
"Chapter "Working with the ctrlX CORE -> Storage media -> SD cards and USB support"