11-01-2020 06:17 PM
I have never been able to SSH into my CtrlX Core Demo. I've tried using PowerShell on Windows with OpenSSH enabled. I've also tried putty. I have the standard boschrexroth user configured on the demo. I always fail with the password for some reason. Is there a setting or security issue I'm missing when trying to SSH? The SSH protocol status in the CtrlX web portal shows activated. Any ideas?
Solved! Go to Solution.
11-02-2020 11:57 AM
Hi,
yes the standard-PW is not working. And in future the SSH connection gets closed soon.
I am going to contact you if you need further details.
bye Jens
11-02-2020 01:50 PM
Hi,
unfortunately this is not 100% correct Jens.
To enable SSH access, a user must be member of the group "sshuser". You can check this via the user's details tab, in this case: Users & Permissions -> Users -> boschrexroth -> Groups. If the box for sshuser is not checked, the user is not allowed to login via SSH.
By default, currently the following settings apply:
Unfortunately - most likely by design, due to security considerations - the SSH server does disclose as few details as possible about the reason why a connection attempt failed. Usually, it just states "Authentication failed".
In future releases, the default behaviour of the system might change in one aspect: SSH might be disabled by default. Nevertheless, as an administrator you always may decide to re-enable SSH via the sidebar entry.
One last remark: Although you are able to access the system via SSH, the boschrexroth user only provides limited access to the system. It does not provide superuser privileges.
Kind regards,
Michael
11-20-2020 06:42 PM
Hello,
For Rexroth application engineers, is there a super user login we are allowed to use to give us higher permissions with SSH?
Thanks,
Brian
11-23-2020 08:32 AM - edited 05-02-2023 07:10 AM
There are no hidden users for internal engineers. There are following options:
EDIT: See this thread for news to this topic.