FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We will start the migration process in one hour.
The community will be then in READ ONLY mode.
Read more: Important
information on the platform change.
06-16-2022 12:42 PM
For supporting MODBUS-TCP, the suggestion was to use the PLC App with CODESYS - Fieldbus communication Add-on, but I did not find one item for Modbus support in the configuration tool.
Is any documentation available to describe this functionality?
Solved! Go to Solution.
06-20-2022 11:24 AM
Hi GBARyder,
maybe this was a missunderstanding.
Modbus-TCP is not a Codesys Addon, you can use directly in PLC Engineering our library CXA_ModbusTCP.
11-03-2022 10:55 AM - edited 11-03-2022 10:56 AM
Dear All,
Customer want to use our CtrlX Core (Modbus TCp IP protocol) connect to BACnet IP via Intesis gateway as link:
Do anyone have experience about this gateway.
Do we need any recheck, @TheCodeCaptain, @CodeShepherd please help
And they ask:
As I check here, there is no limit information:
https://docs.automation.boschrexroth.com/doc/1616011786/il-modbustcpclient/latest/en/
Thank you so much
11-09-2022 08:46 AM
Hello,
I don't know the answers to the questions asked, but I also have an alternative solution. Our XM2 and XM4 controllers support BACnet IP as client and server. A connection between the ctrtlX core and the XM controllers would then also be possible via OPC UA. This could be more powerful than a Modbus/TCP connection.
Regards