FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
10-21-2024 12:59 PM - last edited on 10-21-2024 02:58 PM by CodeShepherd
Hi Karsten, does the platform offer the ability so custom applications can interface with software to generate PLC Code?
does CtrlX have the capability of making simple online changes as other PLCs in the industry?
does CtrlX have the capability of having ethernet / IP slaves such as remote IO?
thanks
Solved! Go to Solution.
10-21-2024 03:19 PM - edited 10-21-2024 04:17 PM
Moved topic to the forum from the ctrlX Store page SDK for ctrlX AUTOMATION.
@mralvarado22 There is a REST API to the ctrlX PLC Engineering, that can be used for creating and manipulating PLC code. See official online documentation "API for ctrlX PLC Engineering" and how to "Use ctrlX PLC Engineering API with Python"
Yes, ctrlX PLC Engineering is supporting online changes, as it is based on CODESYS.
Yes, there can be a EthernetIP scanner be implemented e.g. via CODESYS - Fieldbus Communication.
10-22-2024 04:13 AM
Thank you so much @CodeShepherd ! This helps. I'll review the references you sent and come back to you.
10-22-2024 04:27 AM
@CodeShepherd when you get a minute may you please try this link "API for ctrlX PLC Engineering" and check if it works for you, it didn't work for me thanks ... https://docs.automation.boschrexroth.com/doc/3683011651/api-for-ctrlx-plc-engineering/latest/en/
10-22-2024 08:52 AM
Both links are working fine on my side and opening the same page as it se same link address.
10-22-2024 11:51 AM
10-22-2024 12:45 PM