01-28-2023 07:09 AM
01-30-2023 07:39 AM
See our online documentation for information about SD card and USB usage.
02-01-2023 04:50 AM
Thanks,I will have a try.
02-01-2023 09:16 AM - edited 02-01-2023 09:29 AM
Hi,
In case you're building a custom app the plug should be: removable-media.
If you want to write data from an app to the usb stick you have to:
I suggest you to try first with the official node-red app first.
There are not many apps with this necessity.
Mauro
02-05-2023 09:46 AM
Hello
Is there a detial Operation manual tell me how to step by step to accomplished?
02-06-2023 08:08 AM - edited 02-06-2023 08:11 AM
Did you check manual mentioned above for general usage? Could you tell us from where you like to use the SD-card?
See this topic where different possibilities are listed for general file access.
02-07-2023 02:36 AM
Hello
I want to used ctrlxcore SD-Card just like I used MLC75 PLC CF-Card,when the services guys need to maintenance the machine,They don't use the source PLC code and Drive Configuration files, and a new ctrlxcore can read SD-Card files to restart by automatic.
02-07-2023 08:00 AM
In the MLC the CF card was the main working storage of the control and in the ctrlX CORE there is an internal flash for the system, so it cannot be used exactly the same way. But he µSD card can be used as extension or for restoration. See Topic "Backup/Restore after Hardware Fail" for your use case.
02-08-2023 01:53 AM
02-08-2023 07:11 AM
Should work now. Please try again.
04-24-2023 09:23 AM
Are there any news or can this topic be closed?