FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
04-12-2021 09:19 PM
I have a ctrlX-Core running version 1.6. I'm experiencing a variety of weird issues and would like to reset my PLC. On the Indracontrol MLCs one can hold down a couple buttons and wipe the controller. How would I do the equivalent with my Core?
Solved! Go to Solution.
04-13-2021 07:27 AM
Currently it is not possible to do a factory reset in an easy way. The only possibiltiy is to make a new installation of the core image which can be done by our service departments. But this will delete all stored date (certifications, keys, assertions, ...)
For the future we working on a better solution to do a factory reset over a SD-card / via web interface.
In your case I would recommend first to load a new (empty) configuration. So you can configure your control from the scratch.
Maybe (if you HW can manage this) you can also update to the new version (RM 21.03) available at the collaboration room.
If this will not help you have to contact our service department.
02-21-2022 08:14 AM - edited 10-19-2023 11:35 AM
As an update to this topic:
In the ctrlX CORE Runtime Release notes for RM21.11 (version 1.12) that can be found in the online documenation:
See "ctrlX CORE Runtime, Release Notes XCR-V-0112 --> Important information --> Notes on XCR-V-0112.5"
Or on the collaboration room similar release notes are available, that you can use. Not registered for download yet? Instruction here.
There it's described in the chapter 2.3.1 for real cores, 2.4.1 for virtual cores but for them the easiest way is to simply create a new one in the new installed ctrlX WORKS.
Beware that from the release milestone RM21.11 (version 1.12) all application apps needs a license to be able to run.