cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

How to avoid appData misfitting problems when updating a ctrlX CORE to v1.10

How to avoid appData misfitting problems when updating a ctrlX CORE to v1.10

CodeShepherd
Community Moderator
Community Moderator

How can a customer avoid problems with appData misfitting when updating a ctrlX CORE to the release RM21.07 (v1.10)?

1 REPLY 1

CodeWasi
Occasional Contributor

Setting up a new ctrlX COREvirtual is based on a image and scheduler config which does not fit to your setup by default.

Assuming e.g. the motion app was installed and swichting to RUN-Mode is not possible you may struggle because of misfitting configs.

Either you can configure the avialbable "app-callables" manually or you Reset the configuration by following button under Manage app data

Since the process gets modifcated with the next release we recommend to just click ones the reset-button in the configuation

CodeWasi_0-1627649002561.png

Missfitting Setups - for instance: the installed motion.app is not represented.
Booting the motion will never lead to run, since the callable is not called....

CodeWasi_1-1627649322978.png

After the Reset:

In case the reset is performed - dont care about the intergration:

CodeWasi_3-1627649907472.png

Manually setup as an alternative in general:

Individual setup ot the callable inside the scheduler config. started with +sign

CodeWasi_2-1627649411628.png

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist