FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
08-03-2021 04:45 PM - edited 08-03-2021 04:46 PM
Hello,
I have this error at boot-up after updating core to RM21.7 systems apps and Apps
What is cause ? How to fix this issue ?
Thanks
Solved! Go to Solution.
08-03-2021 07:01 PM
Callable Task was missing in Scheduler. Used "Reset" In Manage App Data to start a new Configuration ( Load Default..) from Scratch. Task are then added automatically
08-04-2021 09:47 AM
It is a known topic because of an update from RM21.03 (v1.8) to RM21.07 (v1.10) and using the old AppData (active configuration).
See also this topic.