09-26-2022 03:58 PM
Hello,
A customer wants the VPN Client app 1.16 version.
But I couldn't find it in the collaboration room for RM22.07 or elsewhere.
Can anyone help? Thanks!
Solved! Go to Solution.
09-27-2022 11:15 AM
Hello LuisCtrL,
VPN Client App 1.16 is not released yet! The app will be released with Patch 2 of V1.16. At the moment, it is planned for mid of October.
09-28-2022 08:21 AM
Thanks Stefan!
Greetings,
Luis
11-23-2022 09:14 AM
Hello StefanH,
The customer has installed the 1.14 app on a Core with 1.16 software and the licensing screen indicates that it is not installed, having access to the VPN in the settings menu.
Any idea why this is happening?
Thanks
11-23-2022 09:21 AM
This is because the WebUI checks the licenses from 1.16 on via an interface of the apps itself. The 1.14 app does not have this interface so this faulty status is shown. This will have no influence to the function.
12-07-2022 02:29 PM