cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

CtrlX core X3 profinet device transition in safe-op

Jesse
Established Member

CtrlX core X3 profinet device transition in safe-op

we got a demo of CtrlX Core X3 with profinet slave ports at xf-23 and xf24. the profinet device app and other apps (version 1.16)were installed and licensed. after having XF23 port configured as profinet device and running the transition status is always at Safe-OP mode. 

Jesse_0-1669643157369.png

when checking the scheduler it shows operating.

Jesse_1-1669643223197.png

since the CtrlX I/Os have not been installed yet the Ethercat Master has an error "Topology not OK"

Jesse_2-1669643399723.png

this is the first time to test X3. does the Ethercat master error affect the profinet status?

then I set up a XM22 as profinet master and loaded the device data file. the master can have the device scanned. after having the settings applied in the project and downloaded it showed module not found.  

Jesse_3-1669643980594.png

from that I can guess the issue is from the CtrlX core X3, but after having most settings checked I haven't seen where to change the profinet settings and how to fix it. let me know if I have missed any settings. 

your help will be appreciated.

 

 

 

8 REPLIES 8
CodeShepherd
Community Moderator

Re: CtrlX core X3 profinet device transition in safe-op

Actually there are technical issues in the prototype version 1.16 of the Profinet device app, so that communication cannot be established. We are actually working on this.

Jesse
Established Member

Re: CtrlX core X3 profinet device transition in safe-op

Thank you for answering that. I was wondering if there were something I did wrong. let's wait an update on that.

CodeShepherd
Community Moderator

Re: CtrlX core X3 profinet device transition in safe-op

Release of the ctrlX Profinet App is now planned for KW3 2023.

Jesse
Established Member

Re: CtrlX core X3 profinet device transition in safe-op

Thank you. that is a good news.

POUL
Member

Re: CtrlX core X3 profinet device transition in safe-op

New app release PROFINET device PND-V-0118.1 in DC APP Pack Paket 18.2 still stay in Safe mode

CodeShepherd
Community Moderator

Re: CtrlX core X3 profinet device transition in safe-op

It is part of the actual pre series app package 1.18.2 that can be found on the collaboration room. Please have a look to the ctrlX Store area here in the forum  for latest information about the app e.g. where to download.

JHU1XI1
Established Member

Re: CtrlX core X3 profinet device transition in safe-op

I have a similar situation. You can delete the PN node and add it again. You can try the following.

CodeShepherd
Community Moderator

Re: CtrlX core X3 profinet device transition in safe-op

I talked to our R&D and there are two main reasons why you could get stuck in safe-op:

  1. IO data settings of the controller side must fit to the slave. When using a XM22 as controller scanning will find the correct IO structure.
  2. There are problems in the Scheduler settings. See Release notes for known ones and how to fix this.
Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist