Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Automatically restore from USB

Automatically restore from USB

aFouraker
Occasional Contributor

Can a core be configured or commanded to automatcially update a controller from USB? The use case would be a field core that needs a plc program update, could this be achieved with USB automatically or thorugh some http requests? 

3 REPLIES 3

Jochen_Mueller
Community Moderator
Community Moderator

Hello Alex

currently we are working on a new function named "Setup". With this function it is possible to

  • load complete core data back to the control
  • updating single apps / app data (like an PLC program)
  • can be done via PC or from a SD-card/USB-stick, ...
  • It is also planned to have a kind of auto-Start. Means you insert the SD-card, switch on th CORE and it start to load....

The first itteration will come with the RM22.03. The most features should be available end of the year.

Regards

Jochen

Hello Jochen_Mueller, 

There are any news about this tpoic please i'm very intersted ? 

Thanks, 

 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist