03-01-2022 11:08 PM
Hello,
When developping locally on PC the IO Manager needs to use ioHandlerOPC.dll this allows to browse and create variables , however when comes the time to publish the app on the ctrlX Core the ioHandlerOPC must be used.
Is there a way to change the OPC source without editing or recreating all variables ?
IO handler config when working on PC
IO Handler config for publishing on the ctrlX core
Solved! Go to Solution.
03-02-2022 09:09 AM
Hello Yul725,
there's no need to use two different IO Handlers. If you just omit ".dll" from the corresponding field it will work on both Windows and Linux systems. There is always only one OPC UA IO Handler available in WebIQ - not two. With ".dll" you explicitly tell WebIQ to load the DLL, which will fail on Linux as there it is a .so file. Omitting the extension will make it work on both systems.
Regards,
Sascha Kimmel
03-07-2022 06:24 PM
Hello,
I started as you wrote with no extension but since I could not get the connexion to the server I read the manual and found that information about the different extensions. I added the ".dll" it worked. When I published the project to the ctrlX It worked only If ".so" extension.
Please let me know What I am doing wrong.
03-08-2022 09:10 AM
Hello Yul725,
if the DLL would not be found on Windows you'd simply not be able to see any of those fields in the IO Handler configuration when selecting the corresponding IO Handler. So we can rule out that this is an issue here on Windows as it would simply show "IO Handler not available" just like when you'd rename that entry:
As you didn't state how you have connected to ctrlX via WebIQ Designer can you please specify if you are connecting directly to ctrlX using the --ws-host parameter or if you have a local instance of WebIQ Server you are using?
Regards,
Sascha Kimmel
03-08-2022 02:18 PM
Hi Sasha,
I did the following tests:
What's next ? I could share my screen on a Teams ?
Thanks!
Gabriel
03-08-2022 02:40 PM
Hello Yul725,
to be able to help you answering my question from before is required: "if you are connecting directly to ctrlX using the --ws-host parameter or if you have a local instance of WebIQ Server you are using"
Regards,
Sascha
03-08-2022 03:09 PM - edited 03-08-2022 03:10 PM
Hi Sascha,
I am using a local instance.I have a developper license on my PC. I am not using the -ws-host...
Regards,
03-08-2022 03:38 PM
Hello Yul725,
thank you for the info. Can you please provide the file %PROGRAMDATA%\WebIQ\connect.log then? You can also do that via a PM.
Regards,
Sascha
03-10-2022 12:00 PM
Hello Yul725,
thank you for providing the log file. There appear to be connection issues with the ctrlX system.
Unfortunately I cannot help you with this but maybe someone from BR can take over this ticket?
[2022-03-08 14:08:08.849119] [ information | ctrlx-CORE] Connected to OPC-UA Server.
[2022-03-08 14:08:08.849119] [ information | ctrlx-CORE] security policy is: Basic256Sha256
[2022-03-08 14:08:08.849119] [ information | ctrlx-CORE] message security mode is: Sign
[2022-03-08 14:13:04.580034] [notification | ctrlx-CORE] Attempting to reconnect to 'opc.tcp://192.168.1.1:4840'.
[2022-03-08 14:13:14.864533] [ error | ctrlx-CORE] Connection error.
[2022-03-08 14:13:14.864533] [ error | ctrlx-CORE] service_type(): OpenSecureChannel
[2022-03-08 14:13:14.864533] [ error | ctrlx-CORE] error(): BadTimeout
[2022-03-08 14:13:14.864533] [ error | ctrlx-CORE] client_side_error(): no
[2022-03-08 15:16:43.268523] [ error | ctrlx-CORE] Connection error.
[2022-03-08 15:16:43.268523] [ error | ctrlx-CORE] service_type(): OpenSecureChannel
[2022-03-08 15:16:43.268523] [ error | ctrlx-CORE] error(): BadCommunicationError
[2022-03-08 15:16:43.268523] [ error | ctrlx-CORE] client_side_error(): no
[2022-03-08 15:16:48.627143] [ error | ctrlx-CORE] Connection error.
[2022-03-08 15:16:48.627143] [ error | ctrlx-CORE] service_type(): ActivateSession
[2022-03-08 15:16:48.627143] [ error | ctrlx-CORE] error(): BadSessionIdInvalid
[2022-03-08 15:16:48.627143] [ error | ctrlx-CORE] client_side_error(): no
Regards,
Sascha