How with WebIQ write OPC-UA objects to ctrlX CORE?

How with WebIQ write OPC-UA objects to ctrlX CORE?

Kostya
Member

Hello.

For example I want to switch motion handler into running state via button. And I think I should write something into "motion/cmd/opstate/Booting" branch in OPC-UA (while core motion handler is in configuration). I have tried writing True and true with type BOOL with no effect. While reading of readable branches (like state of said motion handler) works fine.

3 REPLIES 3

felX_CORE
Member

Hello Kostya,

I tried to solve your problem, but unfortionately it doesn't seem to be so easy.

Motion_Opstate_OPCUA.png

The difficulty seems to be that the opstates are objects and therefore could not be loaded into WebIQ, since WebIQ don't accept objects yet.
Therefore, I also think you need a command with a struct of values to set the opstates and can not change them with a single bool.
You might can solve it with a rest command or over the PLC as support layer in between, but this is just a guess from my side.

I hope I could help you at least a bit further.

-Felix

Is this still an issue or can this topic be closed?

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist