03-31-2023 05:27 PM
Is it possible to create a custom "device" with a specific resolution that can be used in the layout manager? None of the default options match either the exact resolution or the aspect ratio of the WR21 web panels.
Solved! Go to Solution.
04-03-2023 11:52 AM
This is currently not possible with WebIQ. If you only want to use it for the preview (i.e. not for device-specific styling in WebIQ - see the manual for details) - you can simply use the built-in tools of the browser by pressing F12 and then following this tutorial:https://anexia.com/blog/en/chrome-devtools-for-responsive-web-design/
04-03-2023 02:46 PM
Hello webiq-sk,
Thank you for your response. I am aware of the browser developer tools, however this is not as helpful as having a configurable screen size directly in the designer. Hopefully this will be a feature added in future versions of the WebIQ Designer.
09-06-2023 01:32 PM
Hello webiq-sk,
Is ther any change in this topic? It would be helpful if I can adjsut the device properties for easier development.
Thanks, Csaba
09-06-2023 01:52 PM
No change, but noted.