cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Can we export alarm manager entries?

Can we export alarm manager entries?

LunatiX
New Contributor

Is it possible to do a export of the entries of the alarm manager?

4 REPLIES 4

webiq-sk
Frequent Contributor

Hello LunatiX,

you can export/read alarm definitions (which are shown inside the Alarm Manager in WebIQ Designer) using the Server API (Websocket API).

Regards,
Sascha

Hi Sascha

I tried it out with Postman, but I'm not able to establish a WebSocket communication:

LunatiX_0-1647340521796.png

I tried it out also with a chrome extension "Simple WebSocket Client" but also without success.

Additional infos:

  • a WebIQ application is running on the CORE
  • the WebIQ Designer is closed (after a successfull connection with --ws-host=192.168.0.34 --ws-port=10123)

webiq-sk
Frequent Contributor

The error message you are getting is correct. You are not requesting the correct subprotocol "smarthmi-connect"  that is sent in the response headers.

Thanks. With the following settings it works fine:

LunatiX_1-1647362679391.png

After a successfull established communication, I used the user.login function and after that I'm able to use other function.

 

 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist