cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

python.webserver SDK 1.10 Example

python.webserver SDK 1.10 Example

maurusbien
Established Member

Hello,

I tried the python.webserver example from the SDK 1.10 and I was able to snap the example but unfortunately once when I want to open the web page of the webserver on a ctrlX CORE virtual I just get the following screen:

2021-08-24_16h49_36.png

 

The ctrlX CORE virtual is in Operation Mode. When I am trying the hint of the readme.md to take a look into the log of the snap it says, that the webserver is started:

2021-08-24_16h50_07.png

Unfortunately I get no other diagnostics even not in the logbook...

Does this example even should work on the ctrlX CORE virtual?
Are any changes in the package-manifest are necessary because it runs on a virtual ctrlX CORE?

Thanks in advanced!

1 REPLY 1

b3er
Member

I did run into the same issue. For me the problem was that the app was named sdk-py-webserver...
In the

configs/package-assets/rexroth-python-webserver.package-manifest.json

the app was always named rexroth-python-server. When I renamed sdk-py-webserver (in the snap/snapcraft.yaml) it worked (only tested on the real ctrlX)

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist