'ctrlx-datalayer-*.deb': No such file or directory

'ctrlx-datalayer-*.deb': No such file or directory

Tamer
Established Member

Hello,

I have created a fresh instance for the App build environment, and I was following the setup video below step by step, but after executing the './install-sdk.sh' command, I get the below error at the end, it seems that the ctrlx-automation-sdk folder is missing?

I also could not connect to host through the Remote -SSH on Visual Studio, not sure if these two issues are related.

Any ideas would be appreciated, and sorry if these were obvious, I am still starting to play with the SDK and the App build environment.

https://developer.community.boschrexroth.com/t5/Store-and-How-to/Setup-ctrlX-WORKS-App-Build-Environ...

Tamer_0-1662435771333.png

 

2 REPLIES 2

nickH
Community Moderator
Community Moderator

Hello,

it looks like your App Build Environment does not have a network connection, or your App Build Environment didn't have the connection during the first boot. During the first boot many important package get installed. 

I would recommend to create a new App Build Environment and make sure that the virtual environment got a network connection. Also be sure to wait until the App Build Environment shuts down itself. 

When you create the App Build Environment have a look at this box:

nickH_0-1662469425266.png

 

  • Select 'Use HTTP and HTTPS proxy on localhost:3128' if your host is behind a proxy. In this case install and run px.exe before you start the App Build Environment.
  • If your host is not behind a proxy you have to uncheck it.

 

 

Best regards,

Nick

BRamos
Established Member

There is a second step to this.

After making sure the first boot is connected to the internet as mentioned in nickH reply. There is also the issue that the https://api.github.com/users/boschrexroth/ might not be reachable at the moment. This also causes the command to fail.

Please execute the command:

curl -I https://api.github.com/users/boschrexroth/"

And do the installation after there are available request slots. This solution is based on the comment made by @ham1hel in the link: https://developer.community.boschrexroth.com/t5/Store-and-How-to/Setup-ctrlX-WORKS-App-Build-Environ...

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist