04-22-2024 04:21 PM
Hello everyone,
I started working with scheduler from rt SDK, I tried some features and all worked well.
Now I tried to integrate the scheduler (rt SDK) into my existing app when I install the app in the real core, I have the following errors and nothing works.
Can anyone help me with this?
Solved! Go to Solution.
04-25-2024 11:22 PM
Did you get some training about the RT SDK already, as we suggest not to use it without because of the heavy impact the apps will have to the system. See further information in the FAQ for SDK for ctrlX AUTOMATION.
Best would be to get in direct contact with your known application engineer.
04-26-2024 11:30 AM
Problem is already solved. Was necessary to add CMakePresets to my project.