01-25-2024 02:31 PM
Hello,
when I am trying to follow the descriptions within the python and goLang example projects on how to connect to the DL of a virtual CORE, it is not working for me.
First of all, I disabled the check on "SNAP" environment, as in WSL is was always true and returned "ipc://". The string address is not working with any IP I enter. Did anybody of you faced the same issue? It would speed up my development if I could run the code manually first instead of building and deploying the app every time.
Thanks and best,
Karim
Solved! Go to Solution.
01-25-2024 03:00 PM
Hi Karim,
I never worked in a WSL, so I'm not sure if it can be a networking issue in the WSL environment. In a qemu-base environment the connection to a ctrlX CORE virtual works like this:
tcp://<user>:<pw>@<ip-adress-of-ctrlX-CORE>
example: tcp://boschrexroth:boschrexroth@192.168.1.1
tcp://<user>:<pw>@10.0.2.2?sslport=8443
Remarks:
* 10.0.2.2 is the IP address of the host (windows) from the point of view of the QEMU VM. (This is propably different to your WSL)
* 8443 is the host port which is forwarded to the SSL port (=433) of the ctrlX CORE virtual
Best regards,
Nick
01-25-2024 03:12 PM
To add one remark:
I would recommend to use the ctrlX App Build Environment as a build environment. It is integrated in ctrlX WORKS and works similar like the ctrlX CORE virtual. It is a Ubuntu Server machine emulated with QEMU.
Learn how to set it up: here.
01-25-2024 03:32 PM
@nickH Thanks a lot! I used the ctrlX App Build Environment before. Unfortunately, it is failing to build (especially) the goLang examples when datalayer is involved. So I wanted to check if the same is happening on WSL and there it is working - at least the build process.
01-26-2024 08:43 AM
Hi @K-Zanaty
I just tried to reproduce your error. I set up a fresh app build environment with ctrlX WORKS V2.4 ran the following scripts (from the folder scripts): "install-sdk.sh", "install-go.sh" and "install-cpp-aarch64-libs.sh". And I'm able to build the go-samples for amd64 and also arm64.
01-26-2024 10:55 AM
@nickH I can only find V1.20 to download, where do I get V2.4? Is it a pre-release I need to get access to?
In this setup it fails with the messages I post below. I also need to edit the build-*.sh files to execute the snap commands as root. I tried setting up new Build environments multiple times, also reinstalling everything. I am using V1.20.8
2024-01-26 09:49:48.684 executed go version with output go version go1.21.6 linux/amd64
2024-01-26 09:49:48.687 :: + case x86_64-linux-gnu in
2024-01-26 09:49:48.687 :: + go build -buildvcs=false -o ../install/bin/ ./...
2024-01-26 09:49:48.748 :: go: downloading github.com/boschrexroth/ctrlx-datalayer-golang v1.3.0
2024-01-26 09:49:49.384 :: go: downloading github.com/google/flatbuffers v23.5.26+incompatible
2024-01-26 09:50:16.615 :: # datalayer.client/cmd/client
2024-01-26 09:50:16.616 :: /snap/go/10489/pkg/tool/linux_amd64/link: running gcc failed: exit status 1
2024-01-26 09:50:16.616 :: /usr/bin/ld: warning: libcrypto.so.3, needed by /home/boschrexroth/scripts/ctrlx-automation-sdk/samples-go/datalayer.client.simple/parts/client/install/usr/lib/x86_64-linux-gnu/libcomm_datalayer.so, not found (try using -rpath or -rpath-link)
2024-01-26 09:50:16.617 :: /usr/bin/ld: warning: libssl.so.3, needed by /home/boschrexroth/scripts/ctrlx-automation-sdk/samples-go/datalayer.client.simple/parts/client/install/usr/lib/x86_64-linux-gnu/libcomm_datalayer.so, not found (try using -rpath or -rpath-link)
01-26-2024 11:54 AM - edited 01-26-2024 11:55 AM
Hi @K-Zanaty,
V1.20 is the latest LTS (long term support) release, these versions are published once a year end of July. In between LTS versions we got early adopter releases, that are published every 4 months. See more information about our release cycle in: Release cycle of ctrlX OS, apps and engineering software.
If you want to get access to the early adopter releases, see here how to do that: FAQ for ctrlX Store.
You can still use V1.20 SDK and App Build Environment if you like, but there is one issue, when you want to use the App Build Environment and SDK V1.20. See my post in the forum.