Issues when deploying Simulink model to virtual PLC

Issues when deploying Simulink model to virtual PLC

martonv
Occasional Visitor

With the following setup:

  • MATLAB R2022a with Simulink v10.5, Embedded Coder v7.8 and MATLAB Coder v5.4
  • Support Package ctrlX OS Target Simulink V0202 installed
  • ctrlX WORKS v2.4.1 running virtual PLC
  • with Automation Core v2.4.0 and Model Connect v2.4.1

I followed the instructions for the example project cxcStateflow to deploy and monitor via Simulink and the Model Connect app. However, at the 'Build for moitoring' step, I was unable to deploy the code, Simulink returns "ERROR: Failed to send file to the model connect snap" message with no further information.

If I try to manually upload the zip files generated by Simulink, I get the following error message

martonv_0-1714722633056.png

https://developer.community.boschrexroth.com/t5/Store-and-How-to/Modelling-Deploying-and-Running-Sim...

Appriciate any help or suggestions.

 

1 REPLY 1

CodeShepherd
Community Moderator
Community Moderator

Is this still an issue? Have there been a solution? And can this topic be closed?

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist