facing Issue with EXE file creation in Labview with MLPI library

facing Issue with EXE file creation in Labview with MLPI library

samkarshan
Long-established Member

Hello

Customer is using MLPI 1.26.2.0

We are facing Issue with EXE file creation in Labview with MLPI library.

Please find the error message in the attached image.

samkarshan_0-1634971158979.png

 

 

About the Problem.

While runnning in my Labview source code the Program and logic which we build is working fine.

But while dumping the source code into the Windows application (.exe) format we start facing the above error. And further the mlpidll is  added and tried in all combinations yet issue wont resolved.

 

Kindly suggest

 

Thanks and Regards

Samkarshan V

--

1 REPLY 1

MrLurtle
Established Member

Hi,

basically you have to copy the *.dll in the directory of your Executable:

HellCoder_0-1635946142802.png

You can find the *.dll in your installation folder of the MLPI SDK. You have to use the correct dll for x64 or x86 Applications:

C:\Program Files (x86)\Rexroth\MLPI-SDK\01VRS\mlpiCoreClient\bin\win-vs2012-x64

C:\Program Files (x86)\Rexroth\MLPI-SDK\01VRS\mlpiCoreClient\bin\win-vs2012-x86

 

There exist an example in an older version of the MLPI SDK Version 1.11.4.0:

Setup_MLPI_SDK-11140.zip\Setup_MLPI_SDK-1.11.4.0\AddComponents\MLPI_SDK-01VRS.zip\mlpi4LabVIEW\samples\sample - Common MLPI\executable\builds\

You can have a look at this example. 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist