FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
11-09-2023 09:22 PM
I have an application in IndraWorks 14. I would like to number the axis in a specific way that requires the numbering exceed 100 though I will never actually have that many axes in any given system. This makes it easier to maintain a single application with all of the possible options on the machine. When I try and number the axes I am unable to exceed 99 (See image). Is there a way to expand this limit?
Solved! Go to Solution.
3 weeks ago
You can assign other sercos addresses to the axis numbers. As far as I know, this is also possible for three-digit sercos addresses in the valid range. But not for the axis numbers. These are fixed internally.