FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
08-09-2024 05:23 PM
I am able to compare the logic of two PLC applications but would like to compare parameters and device data as well. Is that possible through the indraworks tool set?
Solved! Go to Solution.
08-14-2024 04:50 PM
There are a couple of different comparison tools. What type of parameters and device data are you wanting to compare? I'm assuming you're using IndraWorks Engineering.
08-14-2024 08:32 PM
I will need to test this. The use case is that we have some projects that use the SVN repository to track our projects. If someone goes into the field and does not have access to the server it is easier to compare the new project to the existing, bring in the changes to the revision controlled copy and then push that to the server. The missing piece is parameter changes onsite that are tracked in the application. I think this should solve it, thanks!