cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

HCS01-ERR F8078

HCS01-ERR F8078

JHU1XI1
Long-established Member

Hello,

Driving a third-party linear motor, if it works for a certain distance, an error F8078 will be reported.

Have you ever encountered such a situation.

2 REPLIES 2

Drives_Uwe
Community Moderator
Community Moderator

This indicates a problem on the mechnical side that you need more force at the position where the error shows up or the encoder has certain problems to provide the right signals.

Anyway I guess that you should increase the parameter P-0-0004 (speed controller smoothing time constant) from 300 us to a higher value like 2000 or even 4000 us.

Drives_Uwe_0-1709896461486.png

Best provide a frequency response analysis of the speed loop:

Drives_Uwe_1-1709896606272.png

If you never used this function before you can follow the How-To: https://developer.community.boschrexroth.com/t5/Store-and-How-to/Check-regulation-loop-settings-by-u...

 

 

JHU1XI1
Long-established Member

Hello Drives_Uwe,

After repeated testing, when the speed exceeds 1.5m/s, an alarm F8078 will sound. It was found that the maximum output frequency of the encoder is 20MHz, and the driver can receive a maximum of 10MHz. This may be due to this. After the customer replaced the sine and cosine encoders, everything was normal and could meet the customer's requirement of 2.4m/s.

Thank you for your reply.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist