FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
10-10-2023 01:41 PM
Hello all,
Im currently connecting ctrlX core to HCS02 and can not switch EtherCat to "OP" state as the picture below.
I'm using ctrlX core - X3 with system image is V2.02.4 together with HCS02, firmware version: MPH-08V22-D5-FD. Code failure: 0x0001: Unspecified error. Please give me advise if you have been through this issue. Also please check in attachment for EtherCat configuration too.
Thanks in advance!
Solved! Go to Solution.
10-11-2023 08:43 AM
Moved to corresponding sub forum IndraWorks, IndraControl for MLC/MTX, IndraDrive.
Could you please add a parameter file of the drive with all parameter? I guess there is a configuration error in the drive. Please check the logbook of the ctrlX CORE also.
10-23-2023 04:09 AM
Hello CodeShepherd,
Sorry for my late reply.
Your are right. I loaded parameter on previous with sercos configuration and change protocol to EtherCat. Maybe this cause to error. After reseting them I coud connect. Thanks for your hints.