11-21-2022 06:51 AM - last edited on 11-21-2022 07:53 AM by CodeShepherd
EDIT: Moved to own topic by @CodeShepherd from this one.
I know this is an old post.
but I still have this kind of question.
currently I am doing the DAQ via IoT Gateway, and connect to the drive like HCS01, EFC5610 via S/IP protocol, and it is quite simple, I only need the IP address of the drive and can read parameter via P or S parameters.
considering the PR21 will phase our next year, If I switch the hardware from PR21 to CtrlX, how can I implement the same feature as PR21? especially how can I read data conveniently from HCS and EFC or HMC?
thanks in advance
Solved! Go to Solution.
11-24-2022 10:33 AM
Hello @yaxccha ,
This is not correct! IoT Gateway will be phased out in 2025, not next year!
At the moment, we don´t have a similar solution like DAQ in ctrlX CORE. But we know the issue and thinking about possible solutions.