FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
10-02-2020 03:35 PM - edited 10-02-2020 04:41 PM
I used a ctrlX drive (withcore) and set everything to default.
Installed the motion app and Ethercat app and bootup the system.
Adding a axis and move it is no problem. Added Ethercat master, then use ctrlX I/O for loading the topology.
He a problem shows up. System gets very slow and with scanning I get the following errors.
"The current news channel might not be valid or your Internet connection might be not unavailable...."
Then ctrlX I/O runs, but with connecting:
B
Before the trouble started I used the Tiger app. But I do not think that this has anything to do with this problem.
I tried this with a different (private) notebook. But get the same problem.
Solved! Go to Solution.
10-02-2020 08:03 PM
Moved to ctrlX WORKS.
10-05-2020 10:59 AM - last edited on 10-06-2020 09:51 AM by PedroReboredo
Hello
Please check following points
If you have any problems after this, please leave us a post.
Regards,
Jochen
10-12-2020 09:56 AM - edited 10-12-2020 09:57 AM
I checked everything over and over again.
Finally I found the problem in the Ip addres setting of my Ethernet Adaptor. I work on different systems. Therefore I use different ip settings. The ctrlX was on default 192.168.1.1 I also worked on HMC with 192.168.0.1
My Ethernet Apdaptor was on 192.168.0.123 when the problem occurred.
I could worked on the ctrlX withoud any problem, so the adaptor setting does not give any problem till you use ctrlX I/O for scanning the Ethercat. Then you will find out it wont work.
Setting the adaptor back to 192.168.1.123, the the problem was gone.
10-21-2020 02:35 AM
I've had the same problem before,but I've learned from experience that when I use Ethernet,I check the IP address first.It's become a habit!