06-28-2023 02:37 PM
Hello,
I'm working on an application that is using a Rockwell PLC communicating to a ctrlX core. I'm looking for the EDS files for the ctrlX, to load into Rockwell Studio 5000. Can you tell me where i can download the EDS files please.
Regards
Paul
Solved! Go to Solution.
06-30-2023 08:07 AM
Hi Paul,
EtherNet/IP can be supported on the ctrlX CORE by installing the PLC-integratable packages from CODESYS. EtherNet/IP Scanner or Device can be realized. Find further details here: CODESYS - Fieldbus Communication
If you download the CODESYS EtherNet/IP Adapter from the Collaboration Room. The EDS adapter file is included in the delivery scope.
For further support of the CODESYS - PLC Add-ons contact this sub-forum: CODESYS - PLC Add-ons
Best regards,
Nick
06-30-2023 05:01 PM
Hi Nick,
Thanks. Got it sorted.
Have added some additional infomation on how to create the EDS file and import into Logix Designer.
Paul
07-09-2024 08:51 PM
Hi, Pablo.
Pablo can share the EDS with me since the option to export EDS does not appear. please thanks
07-10-2024 10:21 AM
10-04-2024 04:17 PM
Hi Pablo
Do you have any step-by-step instructions on how to develop the application?
Thanks