03-30-2023 09:54 AM - edited 03-30-2023 09:55 AM
What are the options for connecting two ctrlX COREs to exchange data?
UPC UA, .........
Would it also be possible via WiFi?
Solved! Go to Solution.
03-30-2023 10:51 AM - edited 03-30-2023 10:51 AM
I would sum it up as all TCP based protocols are possible. See also this topic for an overview.
Recommended for fast data exchange between several controls is ctrlX CORE - OPC UA Pub/Sub App.
Wifi in general is also possible but you have to care for stability and traffic.