FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
04-09-2024 02:38 PM
Could you please provide more information on what exactly needs to be done in the custom application in order to use the SocketCAN interface?
Solved! Go to Solution.
04-11-2024 07:10 AM
Moved this topic to the forum from the how to article "Reading CAN bus data into ctrlX CORE". @Sgilk for your information.
Currently there is no way to set up the CAN interface via the ctrlX OS web interface.
When an own snap is created it has to have access to the "network-control" interface via a corresponding slot. This is not auto connected because of security reasons. So three possible ways are available:
$ sudo ip link set can0 type can bitrate 125000
$ sudo ip link set up can
04-11-2024 02:49 PM
A couple of small clarifications on point #3 above.