Possible to read and write S20 Ethercat bus coupler AI-4-I using OPCUA in CtrlX?

Possible to read and write S20 Ethercat bus coupler AI-4-I using OPCUA in CtrlX?

kelvin
Member

Hello Community,

Is it possible to read and write S20 Ethercat bus coupler AI-4-I using OPCUA in CtrlX?

I tried testing using UA Test client, however i could not expand to read and write via UA Test client. (see below.)

Ctrlx_datalayer.JPG

UA.testclient.JPG

Warmest Regards,

2 REPLIES 2

CodeWasi
Occasional Contributor

Hello Kelvin,

the current resolving of the Ecat-DatalayerKnots is limited yet. The implementation does not cover yet the subnotes under instances. Not nice but I case you can live with a workaround inside the PLC. you could make the values available als RTData read and provided as new RT-Variable by the PLC. ( Time delay of 1cycle expected/acceptable?).

CodeWasi_0-1658322153492.png

1.Add the RT-Infos of the AI-channels to the PLC.
2. Provide new vars als RT Vars into the Datalayer (using the pragma declare)
3. copying read value to new var.

CodeWasi_1-1658323037381.png

Unfortunately I can not provide a releasedate for the expected resolving.

OK?

Bye

 

Open
Occasional Contributor

hi @kelvin

In the new ctrlX app (etherCAT and OPCUA Server) and system image version 2.04, you can now read and write the etherCAT IO channels from the OPCUA client.

Open_0-1704866231141.pngOpen_1-1704866313810.png

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist